AKD Drive

In addition to the different views, the WorkBench provides a toolbar and a status bar to display some extra information.

For more details about AKD GUI"Graphical User Interface" A GUI is a type of user interface which allows people to interact with a computer and computer-controlled devices click here

WorkBench Toolbar

The toolbar provides access to the following:

Figure 3-22: AKD Toolbar

Status Bar

The status bar provides the following information on the drive:

AKD Status Bar

Figure 3-23: AKD Status Bar

For the SW and HW enable status indicators, the color code is:

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™